fa_logo

Productos

Industrial robot MELFA Intelligent option MELFA Smart Plus

smart-plus-main-banner

This is an option that brings next-generation intelligence to MELFA industrial robots.

Advanced intelligent functions provide leading-edge functions for all phases of customer's operations, from design and startup through to operation and maintenance.

  1. 1.This is the function that support cell production, using robots to overcome the limitations on lead times, production volumes, and location.
  2. 2.Such as integration functions for the various sensors and autonomous startup adjustment functions.
  3. 3.Utilizing Mitsubishi Electric's proprietary AI technology (Maisart).

Lista de productos

smart-plus-predictive-maintenance
Predictive maintenance function

Failing drive parts are detected before abnormalities in robot behavior become apparent. Downtime of production equipment is reduced.

smart-plus-prevent-maintenance
Preventive maintenance function

Tracking the robot's operating status helps managing the robot's condition. Maintenance is now even more efficient.

smart-plus-enhancement-function
Enhancement function for force sense control

Parameters for the optimum operation pattern are found by training in a short amount of time. Set-up and tact times of a force sensor are reduced.

smart-plus-3d-vision-sensor
MELFA-3D Vision enhancement function

Reduced startup time of the MELFA-3D vision thanks to automatic parameter adjustments which utilize our proprietary AI technology "Maisart".

smart-plus-2d-vision-sensor
2D vision sensor enhancement function

Robot systems can be set up easily using the vision sensor without specialist knowledge.

smart-plus-calibration-assistance
Calibration assistance function

Easy set-up of 2D vision sensors and improved job precision. Time-consuming teaching is automated improving also the accuracy.

smart-plus-coordinated-control
Coordinated control of additional axis

Coordinated operation between the robot and an additional axis makes it possible for the robot to work on workpieces that exceed its operating range.

smart-plus-thermal-compensation
Robot mechanism thermal compensation function

Compensates for thermal expansion of the robot arm to increase position accuracy.


Related Links

fa-e-learning-sm-banner
Powered by Translations.com GlobalLink Web Software