fa_logo

Interfaces hombre-máquina (HMI): GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Recommended functions of GT25 Handy GOT

Sequence program monitor (Ladder)/sequence program monitor (iQ-R ladder)

The GOT can monitor and edit a sequence program in a controller in the ladder format, and also can change current values of devices. When an error occurs, monitor the ladder program and identify the cause of error.
There is no need for a personal computer on the production floor.

Sequence program monitor (Ladder)/sequence program monitor (iQ-R ladder)

System launcher/System launcher (servo network)MECANISMO GOT

A graphical configuration diagram of programmable controller and servo systems indicates module statuses.

System launcher/System launcher (servo network)

Registro de operaciones

The GOT records all the operations performed by operators.
Checking the recorded operation history helps you to identify and analyze the cause of the error occurred due to improper operations, leading to making improvements, preventing reoccurrence, and enhancing traceability.

Registro de operaciones

Grabación de accionamientoMECANISMO GOT

The GOT can be used to display the screen equivalent to the drive recorder of MR Configurator2.
Easily check the servo data (motor current, position command, etc.) on the GOT without using a personal computer.

Grabación de accionamiento

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software