fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Security & Additional System Features

Prevent data alteration with security settings for PDF files
GT Reporting Tool

Having problems?

Having problems?

Can we check the GOT resource data on a personal computer? We need to consider how to prevent data alteration.

GOT will solve your problems!

GOT will solve your problems!

By using GT Reporting Tool on a personal computer, the resource data created with GOT2000 or GT SoftGOT2000*1 can be converted to PDF files. Unauthorized use can be prevented by setting security for PDF files.

*1Restrictions apply to some functions. For the details, please refer to the specification details and restrictions at the bottom of the page.

Function features

Some functions of GT Reporting Tool can be executed with a command line. It is useful for converting multiple files at once because the tool has various functions such as setting a logo and setting a PDF password and digital signature.

Automatic file conversion

The resource data can be converted to PDF files automatically. Files can be automatically converted by setting the network drive*2 as the destination to save the GOT resource data and then setting the network drive as the file server for GT Reporting Tool to access.

*2For the details, please refer to Network drive.

Automatic file conversion

Specification details and restrictions

●Resource data that can be converted to PDF files

Report file (*.G2R)*1, alarm file (*.G2A)*1, logging file (*.G2L), operation log file (*.G2O)

*1GT SoftGOT2000 does not support outputting files of this format.

●Operation with a command line and executable functions

For the details, please refer to the Help for GT Reporting Tool. When installing GT Reporting Tool, the Help for the tool is also stored in the installation folder. Before starting operation with a command line, it is required to install the latest version of Data Transfer Tool.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23 GT21 GS21 SoftGOT*

*Restrictions apply to some functions. For the details, refer to the specification details and restrictions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software