fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Security & Additional System Features

Printing stored data all at once
Printing hard copies and reports

Having problems?

Having problems?

How can I make the printer ready and then print data all at once?

GOT will solve your problems!

GOT will solve your problems!

Files created in the hard copy function or report function can be printed on a printer.
When printing reports, the data can be temporarily stored in an SD memory card or other data storage and printed all at once.

Function features

The hard copy data captured while running GOT or the collected report data can be printed.

Supported printer*1*2

  • Serial printer
  • PictBridge-compatible printer**3
  • Ethernet printer*4
  • *1For the supported printer models, please refer to the Technical Bulletin No.GOT-A-0160-AE (PDF).
  • *2On GT SoftGOT2000, data is output to a printer that is connected to a personal computer.
  • *3Not supported by GT2505, GT25 wide, GT25 handy, GT25 rugged, GT23, GT21, and GS21.
  • *4Supported by GT2104-R and GT2103-PMBD among GT21.

Printing reports at an arbitrary timing

The timing to output reports is as follows. Triggers to output data can be set for each report screen.

GT27 model, GT25 model, GT23 model

  • When trigger condition is satisfied
    Stores the collected data into a temporary file, and collectively outputs the data to a report when the output trigger condition is satisfied.
  • At the time of data collection (only when using a serial printer)
    Outputs the collected data to a report simultaneously with data collection.
  • Report output destination
    Reports can be output to a file in a data storage or to a printer. By using the file print function, the files saved in a data storage can be previewed on GOT and then printed.

GT21 model, GS21 model

  • At the time of data collection (only when using a serial printer)
  • When one page's worth of data is collected (only when using an Ethernet printer)
    Output data when one page's worth of data has been collected.

GT SoftGOT2000

  • When trigger condition is satisfied*1

*1Data cannot be output to a printer directly. Print images (in CSV format) are stored to the virtual A drive of a personal computer once. Output these images in each file to a printer.

*For the necessary option devices, please refer to the "Function list".

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25* GT23* GT21* GS21* SoftGOT*

*Restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software