fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Security & Additional System Features

Identify error cause based on history information
Operation log function

Having problems?

Having problems?

An error occurred due to improper operations, but I do not exactly know why the error occurred...

GOT will solve your problems!

GOT will solve your problems!

*1Not supported by GT21 and GS21.

GOT records all the operations performed by operators. Checking the recorded operation history helps you to identify and analyze the cause of the error occurred due to improper operations, leading to making improvements, preventing reoccurrence, and enhancing traceability.

Function features

GOT records the operation information, such as the "what, when, and how" of an operation performed, in chronological order in an SD memory card or USB memory. Use of the operation log function combined with the operator authentication function records additional information of "who" performed the operation.

*Supported by GT2107-W only among GT21 models.

Easy management for operation log file*1

You can copy and delete an operation log file created by the operation log function and change a file name on GOT without using a personal computer. The operation log file can be converted into a CSV file or UnicodeⓇ text file so that the file can be checked on the personal computer.

*1Supported by GT2107-W only among GT21 models. Changing file name is not supported by GT2107-W and GS21.

Quick check of operation log file

You can select a log from the operation log list and check the detailed information*1. Screen images*2 also help you to identify the improper operation.

  • *1Not supported by GT21 and GS21.
  • *2Not supported by GT21, GS21, and GT SoftGOT2000.
Quick check of operation log file

Coordination with user-created management systems

The operation log records not only the operator names that are used in the operator authentication function but also the character strings stored in an external device. It is easy to coordinate your own user management system and the GOT's operation log.

Coordination with user-created management systems

*For the necessary option devices, please refer to the "Function list".

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23 GT21* GS21 SoftGOT*

*Excluding some models or restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software