fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Maintenance, Troubleshooting and Diagnostics Features

Easy debugging
FA transparent function

Having problems?

Having problems?

It's bothersome to open the cabinet every time I setup or adjust the device. For the safety reason, I don't want to open the cabinet and change cable connections.

GOT will solve your problems!

GOT will solve your problems!

Without opening the cabinet and by only connecting a personal computer to the front USB interface on the GOT, you can use the GOT as a transparent gateway to enable programming, startup, and adjustment of industrial devices.

Function features

By connecting a personal computer to the front USB interface on the GOT, you can use the GOT as a transparent gateway to enable programming, startup, and adjustment of industrial devices.
Users do not have to bother with opening the electrical cabinet or changing cable connections.

Function features
  • *1Not supported by GT2505, GT25 handy, GT23, GT21, and GS21.
  • *2Installation of the wireless LAN communication unit (GT25-WLAN) is required on the GOT.
  • *3For the countries where the wireless LAN communication unit can be used and other details, please see here.
  • *4Not supported by GT23, GT21, and GS21 when the GOT is connected to controllers via Ethernet connection.
  • *5GT21 and GS21 do not support connection to Mitsubishi Electric servo amplifiers.

Transferring GOT project data via a programmable controller

Transfer data from a personal computer to the GOT2000 with a programmable controller acting as a gateway.
Changing project data during startup or maintenance is now easier than ever.

  • *Not supported by GT21 and GS21.
Transferring GOT project data via a programmable controller

Specification details and restrictions

●Supported devices, connection types, and compatible software

For the details, please refer to the relevant product manual.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25* GT23* GT21* GS21* SoftGOT
  • *Restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software