-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
MELSERVO-J5 Series Rotary Servo Motor
Designación del modelo
- Feature
- Especificación
- Normas
- Discontinued
HK-KT Series (Low Inertia, Small Capacity) (Note 2)
- Notas:
- 1.The dimensions are the same regardless of whether or not an oil seal is installed.
- 2.This section describes what each symbol in a model name indicates. Algunas combinaciones de símbolos no están disponibles.
- 3.A geared servo motor with an oil seal installed is not available.
- 4.The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-MT Series (Ultra-Low Inertia, Small Capacity) (Note 2)
Notas:
- 1.The dimensions are the same regardless of whether or not an oil seal is installed.
- 2.This section describes what each symbol in a model name indicates. Algunas combinaciones de símbolos no están disponibles.
- 3.The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-ST Series (Medium Inertia, Medium Capacity) (Note 2)
- Notas:
- 1.The dimensions are the same regardless of whether or not an oil seal is installed.
- 2.This section describes what each symbol in a model name indicates. Algunas combinaciones de símbolos no están disponibles.
- 3.The standard HK-ST G1/G1H servo motors have a keyed shaft (with a key).
- 4.A geared servo motor with an oil seal installed is not available.
- 5.The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-RT Series (Ultra-Low Inertia, Medium Capacity) (Note 2)
- Notas:
- 1.The dimensions are the same regardless of whether or not an oil seal is installed.
- 2.This section describes what each symbol in a model name indicates. Algunas combinaciones de símbolos no están disponibles.
- 3.The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
HK-JT series (Low Inertia, Medium/Large Capacity) (Note 1)NEW
- Notas:
- 1.This section describes what each symbol in a model name indicates. Algunas combinaciones de símbolos no están disponibles.
- 2.The dimensions of the servo motors with functional safety are the same as those of the standard servo motors.
- 3.Available only with the servo motors with the rated speed of 1500 r/min.
- 4.Oil seal is installed in HK-JT series as standard.