fa_logo

Interfaces hombre-máquina (HMI): GOT

Software Features

img-mv-1-sm
MELSOFT GT Works3

Professional designs. Maximized efficiency. Intuitive operations.
All made possible by GT Works3.

This integrated software is used to create professional screen designs for GOTs. Developed with the concepts of simplicity, sleekness, and userfriendliness in mind, this is a powerful tool that pushes boundaries and delivers endless design possibilities.

  • Feature
  • Especificación
  • Normas
  • Discontinued

Support maintenance

GOT offline monitor

The GOT offline monitor graphically displays device values of the data (recording file) that was recorded by the system recorder before and after a problem occurrence on a personal computer.
Since the operation screen and the program having the same time stamp can be reproduced along with the operation of the seek bar on GX Works3, the actual operation and the state of the equipment can be checked simultaneously, thus helping to identify the cause of the problem quickly.

GOT offline monitor

Seek bar

Seek bar is the function to specify the index (consecutive number that is recorded for each scan of the recording file) of the data to monitor.
Operating the slider on the seek bar enables to jump to the event information of the specified index or to check the data by synchronizing the time with the GOT offline monitor.

Resource file viewer

The resource file viewer displays the operation history and the alarm history from the resource files recorded on GOT.
By synchronizing the time between the seek bar of the offline monitor (GX Works3) and the events (operation history, alarm history) on GOT, the relationship between the event data before and after an alarm occurrence and the flow of a program can be checked.

  • *Not supported by GT21 and GS21.
Resource file viewer

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software