fa_logo

Interfaces hombre-máquina (HMI): GOT

Software Features

img-mv-1-sm
MELSOFT GT Works3

Professional designs. Maximized efficiency. Intuitive operations.
All made possible by GT Works3.

This integrated software is used to create professional screen designs for GOTs. Developed with the concepts of simplicity, sleekness, and userfriendliness in mind, this is a powerful tool that pushes boundaries and delivers endless design possibilities.

  • Feature
  • Especificación
  • Normas
  • Discontinued

Support globalization

Speech synthesis function

Just enter arbitrary text in GT Works3 to create a sound file. It is easy to create a sound file of a message that is needed to output sound on GOT. The speaker (female/male), language, speed, pitch, and volume of the voice can be set. Messages can be created in 6 languages and you can create the sound notification system in multiple languages.

  • *To register or update messages, GT Works Text to Speech License (SW1DND-GTVO-M) is required.
Supported language
Image of creating a sound file (message)
Image of creating a sound file (message)

Procedure: [Common] → [Sound] → [Sound File List]

Cambio de idiomas

Create comments of different languages, save them in separate columns, and you can switch languages easily just by switching column numbers. In addition, the character strings of switches and lamps can easily be converted from the Text or Text Figures into Comments. This makes it easy to upgrade screens to display multiple languages.

Cambio de idiomas

Procedure: [Common] → [GOT Environmental Setting] → [Language Switching]

FA Term Translation Tool

This is the software to translate comments (words, sentences) that are used in MELSOFT applications including GT Works3. The software uses the FA Term Translation Dictionary provided by Mitsubishi Electric. You can use the software even when your computer is not connected to the Internet. In addition, it is possible to create your own dictionary and switch dictionaries depending on your needs. The software supports creation of multiple language screens.

FA Term Translation Tool
GT Works3

• Starting FA Term Translation Tool

Procedure: Windows® menu → [MELSOFT] → [FA Term Translation ToolFA Term Translation Tool]

Specification details and restrictions

● Compatible language
•Japanese → English, Chinese (Simplified), Chinese (Traditional), Korean , Thai
•English, Chinese (Simplified), Chinese (Traditional), Korean , Thai → Japanese

● Supported OS (Japanese version, English version)
Microsoft® Windows® 11
Microsoft® Windows® 10

● About this tool
Translation by FA Term Translation Tool is a mechanical translation. Use this tool as a tool to support translation.

● How to obtain this tool
This tool is included in the MITSUBISHI ELECTRIC FA Library DVD of GT Works3 Version 1.130L or later.
Comuníquese con su oficina de ventas local para obtener más información.

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software