fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Startup/adjustment

Parameter settings (simple mode)

  • CASE1
  • CASE2
  • CASE3
  • CASE4
  • CASE5
GT27 GT25 GT23*2 GT21*2 GS21*2 SoftGOT*2*3

Reto

We want to set the parameters without opening the control panel!

Reto

Soluciones

GOT Drive solves your problems

Easily adjust parameters with the GOT
Use the GOT on the front of the control panel to adjust the inverter's simple mode parameters. The parameter names can be confirmed on a list, so the required parameters can be easily found and set.

Soluciones

For the details, please refer to "Parameter recipe".

  • *1Sample screens (VGA) are available. The screen image is the sample screen of FR-A800-E for CASE 1. The screen image differs from the one for FR-E800 and CASE 4.
  • *2Sample screens are not supported by GT23, GT21, GS21, and GT SoftGOT2000.
  • *3Supported by GT SoftGOT2000 (Multiple channels) only.

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software