fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Soluciones remotas basadas en la red GOT

Remote monitoring with SoftGOT
SoftGOT-GOT link function

Having problems?

Having problems?

A problem occurred at the shop floor.
Can I check the situation in my office?

GOT will solve your problems!

GOT will solve your problems!

Without creating screens for remote monitoring, check the shop floor on GT SoftGOT2000 by reading project data from GOT at the shop floor.

Function features

Read project data from the GOT connected to GT SoftGOT2000 via Ethernet, and you can monitor the devices that are connected to the GOT on different screens from the one shown on the GOT.

  • *A separate license key (GT27-SGTKEY-U) is required.

Safe with security and exclusive control

Exclusive control of authorization prevents accidents that might be caused by simultaneous operations in the same network. The exclusive control can be enabled/disabled for each screen. (GOT network interaction)
Set passwords to the GOT project data and prevent invalid access.

GOT network interaction

Specification details and restrictions

  • *For the necessary option devices, please refer to the "Function list".

●Supported devices and connection types

The devices supported by the SoftGOT-GOT link function varies depending on the connection types. For the details, please refer to the relevant product manual.

●Precautions for safe use

When the SoftGOT-GOT link function is used to perform remote control of control equipment, the field operator may not notice the remote control, possibly leading to an accident. In addition, a communication delay or interruption may occur depending on the network environment, and remote control of control equipment cannot be performed normally in some cases. Before using the above functions to perform remote control, fully grasp the circumstances of the field site and ensure safety.

●Functions that can be used in GT SoftGOT2000

In GT SoftGOT2000, some functions available in GOT2000 series cannot be used. For the details, please refer to the relevant product manual.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23 GT21 GS21 SoftGOT

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software