fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Soluciones remotas basadas en la red GOT

Operate the PC from a remote GOT
Función de operación de computadora personal remota (Ethernet)

Having problems?

Having problems?

How can I view manuals and drawings in a personal computer in my office from the shop floor?

GOT will solve your problems!

GOT will solve your problems!

On GOT at the shop floor, you can operate a personal computer in a remote location and view manuals and drawings in the computer. Connecting a USB mouse/keyboard to the front (or rear) USB interface makes it easier to operate the personal computer.

Function features

Connect GOT at the shop floor to a personal computer in a remote location via Ethernet. This allows you to remotely operate the personal computer and view manuals and access the web browser on the computer*1.
The screen of a personal computer, which is playing back a video feed, can be displayed on GOT by setting the remote personal computer operation function license (paid) on the GOT.*1
In addition, if a setting application is built in a camera, adjustment (such as zoom and rotation) can be done and the camera can be operated from a personal computer on the network.

  • *1A separate license (GT25-PCRAKEY-) is required.
Video playback and camera settings/operation are possible only with Ethernet connection

Specification details and restrictions

  • *For the necessary option devices, please refer to the "Function list".

●Validated VNC server

Please refer to the Technical Bulletin No. GOT-A-0110-E (PDF).

●Precautions for safe use

When the remote personal computer operation function (Ethernet) is used to perform remote control of control equipment, the field operator may not notice the remote control, possibly leading to an accident. In addition, a communication delay or interruption may occur depending on the network environment, and remote control of control equipment cannot be performed normally in some cases. Before using the above functions to perform remote control, fully grasp the circumstances of the field site and ensure safety.

Recommended industries

Electronics F & B Plant

Supported GOT types

GT27 GT25 GT23 GT21 GS21 SoftGOT

Supported devices

PLC Servo Inverter Robot CNC
banner_selection_tool_en

Related Links

Powered by Translations.com GlobalLink Web Software