fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Sophisticated Programmable Controller Interactive Features

Support FXCPU maintenance
FX list editor function & FX ladder monitor function

Having problems?

Having problems?

The system has been changed at the shop floor. I need to change sequence programs of the MELSEC-F Series programmable controller.

GOT will solve your problems!

GOT will solve your problems!

Sequence programs of the MELSEC-F Series programmable controllers can be edited in the list (command) format. Minor program changes can be applied even without a personal computer or a peripheral device.

Function features

You can easily edit and monitor sequence programs without preparing any peripheral devices other than the GOT.

FX list editor

Just by simple key operations you can check, partially correct, change, or add parameters or sequence programs of an FXCPU.

  • *Supported by GT2107-W and GT2104-R among GT21.
  • *Not supported by GT25 wide models.
Example of changing sequence program commands

Monitor de escalera FX

The MELSEC-FX list editor can be opened from the FX ladder monitor screen with a single touch operation. You can edit sequence programs while checking the ladder diagram.
You can also display the list screen from the step line displayed in the ladder monitor.

  • *Not supported by GT23, GT21, and GS21.
Monitor de escalera FX

Specification details and restrictions

<FX list editor>

●Target models

FXCPU (FX3U, FX3UC, FX3G, FX3GC, FX3S)

●Supported connection types*1

Ethernet connection*2, direct CPU connection (serial)

  • *1For details on the connectable models for each connection type, please refer to the "Connectable model list" in the GOT2000 Series/GOT SIMPLE Series catalog.
  • *2When the CC-Link IE Field Network Ethernet adapter module is used, the FX list editor cannot be used.

●Functions

Writing sequence programs, setting parameters, PLC diagnostics, registering keywords, etc.

<FX ladder monitor>

●Target models

FXCPU (FX3U, FX3UC, FX3G, FX3GC, FX3S)

●Supported connection types*1

Ethernet connection, direct CPU connection (serial)

  • *1For details on the connectable models for each connection type, please refer to the "Connectable model list" in the GOT2000 Series/GOT SIMPLE Series catalog.

●Functions

Search operation, display switching, test operation*2*3, hard copy

  • *2Present values of V and Z cannot be changed.
  • *3Set values of T and C cannot be changed.

Recommended industries

Electronics F & B

Supported GOT types

GT27 GT25* GT23* GT21* GS21* SoftGOT
  • *Excluding some models or restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software