fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

GOT Drive Control (Inverter) Interactive Solutions

Support maintenance of inverters
Transparente de FA
MECANISMO GOT

Having problems?

Having problems?

We want to perform debugging smoothly!

GOT will solve your problems!

GOT will solve your problems!

By connecting a personal computer with the GOT's USB interface, the inverter can be programmed, started up, and adjusted via GOT. There is no need to open the control panel and change the cable.

  • *1Some system configurations are not supported. For the details, please refer to the connection manual.
  • *2Installation of the wireless LAN communication unit (GT25-WLAN) is required on the GOT. The unit cannot be used with GT2505, GT25 handy, GT23, GT21, and GS21 models. For the countries where the wireless LAN communication unit can be used and other details, please refer to the "Product list".

Specification details and restrictions

  • ●Target models

FR-A800(-E), FR-A800-GF, FR-E800(-E), FR-F800(-E), FR-E700(-NE), FR-D700, FR-A800(-E)-CRN, FR-A800(-E)-R2R, FR-A800(-E)-LC

  • ●Supported connection types*1

Connection via a programmable controller, connection via CC-Link IE Field Network master or local station module

  • *1For details on the connectable models for each connection type, please refer to the "Connectable model list" in the GOT2000 Series/GOT SIMPLE Series catalog.

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25* GT23* GT21* GS21* SoftGOT
  • *Excluding some system configurations or restrictions apply to some functions. For the details, please refer to the connection manual.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software