fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Data Handling Features

Send and retrieve files between GOT and PC
Función de transferencia de archivos

Having problems?

Having problems?

How can I check daily production results?

GOT will solve your problems!

GOT will solve your problems!

By using GOT, production results can be stored on the GOT's SD memory card or USB memory and sent to a personal computer or the USB memory on the front face of GOT. The GOT can also receive production instructions from the personal computer.

Function features

Files stored on the GOT's SD memory card or USB memory can be transferred easily.
Network drive can be used as the transfer destination.

FTP transfer

By using GOT, files stored on the GOT's SD memory card or USB memory can be sent to or received from an FTP server (personal computer). File transfer triggers (sampling, bit rise, etc.) can be used to set file transfer timing.

  • *Supported by GT2107-W, GT2104-R, and GT2103-PMBD among GT21 models.
FTP transfer

GOT internal transfer

Files stored on the SD memory card or USB memory connected to the back side of GOT can be transferred to the USB memory on the front face of the GOT so that data can be obtained easily.

  • *Not supported by GT21 and GS21.
GOT internal transfer

File transfer using a network drive

The GOT data stored in a file server (personal computer) connected by Ethernet can be transferred to an FTP server (personal computer), or the data can be directly transferred between the GOT and the file server (personal computer).

Specification details and restrictions

  • *For the necessary option devices, please refer to the "Function list".

●Validated FTP servers and clients

Please refer to the Technical Bulletin No.GOT-A-0171-C (PDF).

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma Plant

Supported GOT types

GT27 GT25 GT23* GT21* GS21* SoftGOT
  • *Excluding some models or restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software