fa_logo

Human-Machine Interfaces(HMIs)-GOT

Serie GOT2000

img-mv-1-sm
  • Feature
  • Especificación
  • Normas
  • Discontinued

Data Handling Features

Support management of on-site data
File manager function

Having problems?

Having problems?

How can I make backup of alarm and logging data? It's bothersome to back up data separately.

GOT will solve your problems!

GOT will solve your problems!

Folders and files are shown in a list on a graphical screen so that it is easy to copy them as needed.

Function features

Check the folders and files that are stored on the GOT's SD memory card or USB memory, and copy or delete them in the list.

File manager function

Graphical list display

File types can be identified with icons at a glance.

Supporting network drive

Since the GOT files can be directly copied or moved to the network drive, data can be backed up easily.

Various file operations

Copy, delete, move, rename, or create files and folders. Multiple selection of files and folders is also possible.
Files can be operated also in mobile screens using the GOT Mobile function.

Checking available space in drives

Easily check available space in the drives.
It is useful when saving cumulative data such as logging and hard copies.


  • *For the necessary option devices, please refer to the "Function list".

Recommended industries

Automotive SEMICON, LCD Electronics F & B Pharma

Supported GOT types

GT27 GT25 GT23* GT21 GS21 SoftGOT
  • *Restrictions apply to some functions. For the details, refer to the function descriptions above.

Supported devices

PLC Servo Inverter Robot CNC

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software