-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
Motion Control Software SWM-G
Características
- Feature
- Especificación
- Normas
- Discontinued
Concepto
Covering a Wide Range of Multi-Axis Applications
- SWM-G Motion Control Software is available in 16 to 128-axis control models, enabling multi-axis synchronization of various scales of machines.
- A CPU core of the industrial personal computer is assigned for running SWM-G processing, and that enables SWM-G to perform a high-speed, real-time operation without being affected by the operation on Windows®.
Reduced Machine Design and Startup Time
- The integrated test tool SWM-G Operating Station covers the development processes of SWM-G from design to simulation, contributing to reduction in the total cost of ownership.
- The Operating Station enables users to check the communication settings and status of the master/remote stations, leading to reduced design time.
Single-axis control
Master station communication monitor
Maintenance Solution by MELIPC with SWM-G installed
When SWM-G is installed and operated on the MELIPC (industrial personal computer), the system offers a powerful maintenance solution utilizing the Edgecross-compatible software.
-
[Predictive/preventive maintenance]
-
- The user application collects data of machine diagnosis function, etc. from MR-J5-G through the communication API of SWM-G.
- The MELIPC analyzes the collected data by using the Edgecross-compatible real-time data analyzer.
-
[Corrective maintenance]
-
- SWM-G collects data from the drive recorder of MR-J5-G through TCP/IP communications, which reduces troubleshooting time.
Características
Installed on a personal computer, SWM-G Motion Control Software can perform motion and network control.
- Supports a CC-Link IE TSN servo control system with the personal computer where RTX64 (real-time extension) is installed.
(RTX64 is included with SWM-G.) - Meets various application needs by offering various types of motion control, such as positioning, synchronous, cam, speed, and torque control using API library for motion control.
- Utilizes network control to connect and set various device stations (remote I/O modules, etc.) and TCP/IP devices.
Motion Control Software *1
SWM-G*3
- Número máximo de ejes de control: 128
- Minimum operation cycle *2: 125 μs
- Programming language: Visual C ++®
USB key for Motion Control Software
- MR-SWMG16-U: 16 axes MR-SWMG32-U: 32 ejes
- MR-SWMG64-U: 64 axes MR-SWMG128-U: 128 ejes
- *1.SWM-G Motion Control Software includes SWM-G Engine, SWM-G API, Network API, SWM-G Operating Station, and Real Time OS (RTX64).
- *2.The minimum operation cycle depends on the number of control axes and the CPU of the personal computer.
- *3.SWM-G-N1 is also compatible with EtherCAT®.
- *4.A USB key (license) is not required for the free trial version SWM-G-W. To obtain SWM-G-W, contact your local sales office.
Numerous Motion Control Functions
Control de posicionamiento
In this method, an axis can be accelerated gradually through adjusting jerk so that the vibrations of the machine can be minimized.
In the example above, the constant positive jerk is applied at the start of the operation to achieve smooth acceleration.
When the axis is shifted to the constant-speed operation, the same amount of negative jerk is applied.
Ajustando el jaloneo de este modo se consigue una aceleración/desaceleración suave, al tiempo que se acorta el tiempo que se tarda en alcanzar la velocidad objetivo.
La velocidad crea una forma de curva en S.
The triggered motion is a type of command that delays the execution of the motion command until the specified trigger condition is satisfied.
Axes can be started automatically based on the specified conditions by using this command, reducing the cycle time of conveyor systems, etc.
In the operation example above, right after the axis 2 starts execution of normal motion commands, the axis 1 executes the triggered motion command (delaying the execution of the command until the condition is satisfied).
When the condition is satisfied (start trigger ON) during the axis 2 operation, the axis 1 starts executing the motion command.
Motion Control Software enables tandem operation where the same commands can be outputted to master and following axes.
After the master and following axes pass their respective dogs, the gantry home position return stops both of the axes at the Z-phase of the master axis.
This method enables two or more axes to execute home position return simultaneously, supporting gantry systems.
A Wide Variety of Features
The hot connect enables a topology change during operation without requesting a communication stop.
The user application disconnects and reconnects the network through API library.
The controller obtains the status data of servo amplifiers, such as machine diagnosis information and encoder temperature,
via CC-Link IE TSN. This enables visualization of machine status.
The output signal is turned on when a specified condition is satisfied. This function can be used as an alternative to a limit switch.
The current value of the servo motor can be read when the touch probe signal is inputted.
Software and hardware touch probes are available.
Select the touch probe according to your application.
The set offset is applied at regularly spaced command positions. The position error of ball screws can be compensated, improving the operation accuracy.
The set offset is applied when the axis changes the travel direction.
The backlash of ball screws can be compensated, which improves operation accuracy of machines.
The controller offers 24 types of acceleration/deceleration methods, such as trapezoidal, S-curve, jerk ratio, parabolic, sine curve, time acceleration trapezoidal, etc.
Select the method according to your application.
Integrated Test Tool SWM-G Operating Station
This tool provides a variety of features - parameter settings required for application development and the test operation for JOG, inching, and positioning operations. In addition, each axis status and sampled waveforms can be displayed to help user check the start timing and the operation pattern.
[Parameter setting]
- Set/check parameters of each axis on the list.
- Import/export a setting file from/to the personal computer.
[Communication setting]
- Set IP address, axis No., and communication cycle of remote stations.
- Import/export a setting file from/to the personal computer.
- Remote stations are automatically set depending on the communication status.
[Communication monitor of master station]
- The communication monitor shows a list of communication setting of the master station.
- Check the communication status on the system status.
[Communication monitor of remote stations]
- Check the network status and IP address of remote stations.
[Details of remote station status]
- Check details of network status of remote stations, and perform a communication test.
[Single control]
- Perform a test operation for single control.
- A repeat operation is available, which is often used for a test operation.
Multiple Servo Amplifier Settings and Adjustments
MR Configurator2 enables users to easily set and adjust multiple servo amplifiers through CC-Link IE TSN which enables mixing of TCP/IP communication and other communications.
Using MR Configurator2 with the integrated test tool, users can adjust servo amplifiers while checking the servo amplifier communication status.
- Supports MR-J5-G
- Manages a multi-axis system as one project
- Parameters and the machine diagnosis can be set for all axes in a batch on MR Configurator2.
*MR Configurator2 is not included with SWM-G Motion Control Software.
Programa de muestra
This tool provides a variety of features - parameter settings required for application development and the test operation for JOG, inching, and positioning operations. In addition, each axis status and sampled waveforms can be displayed to help user check the start timing and the operation pattern.
Sample Libraries
API library for SWM-G Motion Control Software.
- ■API Library Linked with SoftGOT
-
- The API library enables users to easily exchange data of SWM-G Motion Control Software and SoftGOT2000.
- ■API Library Linked with Mitsubishi Electric Products
-
- The API library enables users to set parameters for CC-Link IE TSN-compatible analog I/O modules and servo amplifiers
(MELSERVO-J5 series).
- The API library enables users to set parameters for CC-Link IE TSN-compatible analog I/O modules and servo amplifiers
Redes integradas abiertas en una empresa de fabricación
CC-Link IE TSN admite comunicaciones TCP/IP y las aplica a arquitecturas industriales a través de su compatibilidad con TSN que permite comunicaciones en tiempo real.
Gracias a su arquitectura de sistema flexible y sus amplias funciones de configuración y resolución de problemas, CC-Link IE TSN es ideal para construir una infraestructura de IIoT en una empresa de fabricación.
- *TSN: Time-Sensitive Networking
- *IIoT: Internet industrial de las cosas
Servoamplificador MELSERVO-J5/MELSERVO-JET
Los servoamplificadores líderes de la industria de alto rendimiento de la serie MELSERVO-J5 cuentan con un motor de control único que ahora es más potente que nunca.
Estos servoamplificadores pueden conectarse a CC-Link IE TSN para llevar a cabo un control de alta velocidad y alta precisión.
Cada servoamplificador multieje acciona un máximo de dos o tres servomotores (según el modelo de servoamplificador elegido), lo que simplifica el cableado y habilita una máquina compacta a un costo menor.
Los servoamplificadores de alto rendimiento de la serie MELSERVO-JET cuentan con un motor de control único que ahora es más potente que nunca.
Estos servoamplificadores pueden conectarse a CC-Link IE TSN para llevar a cabo un control de alta velocidad y alta precisión.
Los servoamplificadores admiten servomotores lineales además de los motores giratorios.
El MR-JET-G-N1 admite EtherCAT®.
Especificaciones
Módulo Motion | |||||
---|---|---|---|---|---|
SWM-G(-N1)*2 | |||||
Número máximo de ejes de control | 16 axes, 32 axes, 64 axes, 128 axes | ||||
Ciclo de comunicación (operation cycle settings) [μs] |
125, 250, 500, 1000, 2000, 4000, 8000 | ||||
Red | CC-Link IE TSN, EtherCAT®*2 | ||||
CC-Link IE TSN class | B | ||||
Especificaciones de comunicación | Mixture of hot connect, SDO communication, TCP/IP communication | ||||
Development environment | • Microsoft® Visual Studio® 2017, 2019 • Programming languages supported by API library: C/C++, .NET (C#, VB.NET, etc.) |
||||
Funciones | Método de control | Position, speed, torque | |||
Posicionamiento |
Up to 128 axes simultaneously (absolute value command, relative value command), Override is possible |
||||
Aceleración/desaceleración processing |
Trapezoidal, S-curve, jerk ratio, parabolic, sine, time acceleration trapezoidal, etc. (24 types in total) |
||||
Interpolation | 2- to 4-axis linear interpolation, 2-axis/3-axis circular interpolation, 3-axis helical interpolation, PVT | ||||
Continuous path | Combination of linear and circular interpolation, spline interpolation, pre-read speed automatic control, linear/circular continuous path with rotation stage | ||||
Operación JOG | Proporcionado | ||||
Real-time control | Event, triggered motion, position synchronous output | ||||
Control sincrónico | Simple synchronization, synchronous gear ratio, synchronous phase offset, synchronous compensation, dynamic establishment/cancellation of synchronization, multiple pairs (up to 64 pairs) of synchronization between 1 axis and multiple axes (synchronous group) |
||||
Electronic cam | Cam curves of eight systems can be defined, cam curve per communication cycle, phase operation, clutch |
||||
Home position return *1 | Home position return using the Z-phase, home position sensor, limit sensor, limit proximity sensor, external input signal, mechanical end, and gantry axis can be performed. |
||||
I/O size | Entrada: 8000 bytes, output: 8000 bytes | ||||
Función de compensación | Backlash/pitch error compensation, plane strain (straightness) compensation | ||||
Auxiliary function | Touch probe, logging |
- *1.SWM-G does not support the home position return mode of the servo amplifier.
- *2.SWM-G-N1 is also compatible with EtherCAT®.