fa_logo

Interfaces hombre-máquina (HMI): GOT

Software Features

img-mv-1-sm
MELSOFT GT Works3

Professional designs. Maximized efficiency. Intuitive operations.
All made possible by GT Works3.

This integrated software is used to create professional screen designs for GOTs. Developed with the concepts of simplicity, sleekness, and userfriendliness in mind, this is a powerful tool that pushes boundaries and delivers endless design possibilities.

  • Feature
  • Especificación
  • Normas
  • Discontinued

Convey information easily and reliably with sound

GT Works3 can now be used to synthesize speech data. Sound files can be created easily.

Convey information easily and reliably with sound

Support sound file creation

Speech synthesis function*1

NUEVO

Just enter text in GT Works3 to create a sound file of a message. (Up to 500 files can be registered.) Messages can be created in 6 languages and you can select the speaker (female/male) for each language. In addition, using FA Term Translation Tool*2 together can reduce time for multi-language screen creation and support globalization of the system.

  • *1GT Works Text to Speech License (SW1DND-GTVO-M) is required separately.
  • *2This tool is included with GT Works3. For more details, please refer to the "FA Term Translation Tool" or contact your local sales office.
Supported language
Image of creating a message

Enhanced playback functions of sound files

Multiple files can be set and played back consecutively (up to 16 files).
The playback time is now longer than before so that various messages can be used.

Enhanced playback functions of sound files

Easily set consecutive playback list (by switch operation or trigger action)

In GT Works3, just specify the files in the playlist in the order of your preference and the files are played back consecutively.

Easily set consecutive playback list (by switch operation or trigger action)
Easily set consecutive playback list (by switch operation or trigger action)

Cancel or mute the sound while it is being played back

After checking the situation, you can stop or mute the sound while it is being played back so that you do not need to worry about annoying other operators.

Checked, OK!

Sound notification is useful at the worksite

Use message, sound effect, or melody to notify occurring events

When an alarm occurs, outputting a warning message or a warning sound can reliably convey the information to the operators who are working away from the GOT. It is also usable while screen saver is active. Quickly notify the alarm information and the error cause of the equipment to reduce the downtime of the system.

Playable Sound file types
Use message, sound effect, or melody to notify occurring events

Funciones adicionales

Even if multiple errors occur, playback all messages

If multiple errors occurred simultaneously, GOT saves up to 16 data and notify all events. There is no need to worry about missing some occurred events.

Even if multiple errors occur simultaneously…
Up to 16 data can be saved

Consecutive playback reduces data size

You can extract common parts and register them as separate sound data to avoid saving duplicate data and reduce data size. To change messages, simply change the combination.

Consecutive playback reduces data size

Useful tips about using sound notification

Change touch sound depending on the situation

The touch sound can be changed depending on the worksite situation or the operator's preference.

Touch sound for various situations
Touch sound for each operator

Use as the sound guidance when touching a switch

When touching a switch, a message guides you to the next operation and notifies cautions so that you can avoid operation mistakes in advance.

Use as the sound guidance when touching a switch

Announce a message in various languages sequentially

When there are operators who understand different languages, you can convey necessary information correctly to every operator.

Announce a message in various languages sequentially
Announce a message in various languages sequentially

Specification details and restrictions

For the supported connection types and necessary option devices, please refer to the relevant product manual.

Related Links

banner_selection_tool_en
Powered by Translations.com GlobalLink Web Software