-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
Human-Machine Interfaces(HMIs)-GOT
GT SoftGOT
- Feature
- Especificación
- Normas
- Discontinued
Contenido
Entorno de funcionamiento
Artículo | Descripción |
---|---|
Computadora personal | Personal computer that Windows® runs on. MELIPC (MI5122-VW, MI3321G-W*9, MI3315G-W*9, MI2012-W, MI2012-W-CL)*10 |
OS *1*2*3*4*11*12 |
Microsoft® Windows Server® 2019 Standard (64 bit) *13*16 Microsoft® Windows Server® 2016 Standard (64 bit) *16 Microsoft® Windows® 11 Education (64 bit) *8*16 Microsoft® Windows® 11 Enterprise (64 bit) *8*16 Microsoft® Windows® 11 Pro (64 bit) *8*16 Microsoft® Windows® 11 Home (64 bit) *8*16 Microsoft® Windows® 10 Enterprise (64 bit/32 bit) *16 Microsoft® Windows® 10 Pro (64 bit/32 bit) *16 Microsoft® Windows® 10 Home (64 bit/32 bit) *16 Microsoft® Windows® 10 IoT Enterprise 2021 LTSC (64 bit) *7*8*17 Microsoft® Windows® 10 IoT Enterprise 2019 LTSC (64 bit) *7*8*17 Microsoft® Windows® 10 IoT Enterprise 2016 LTSB (64 bit) *7*8*17 |
CPU | Windows® 11: 64 bit-compatible processor with dual-core or more or System on a Chip (SoC) *14 Other than Windows® 11: Intel Core 2 Duo Processor 2,0 GHz or more recommended *14 |
Memoria | For Windows® 11: 4 GB or more recommended For 64-bit OS other than Windows® 11: 2 GB or more recommended For 32-bit OS other than Windows® 11: 1 GB or more recommended |
Pantalla | Resolution XGA (1024 × 768 dots) or higher |
Hard disk space*5 | For installation: 5 GB or more recommended
For execution: 512 MB or more recommended |
Color de la pantalla | High Color (16 bits) or higher |
Hardware | GT27-SGTKEY-U (license key (for USB port)) |
Otras opciones de software | The following software is required to create the project data.
• GT Designer3 Version1.100E or later *6
The following software is required for interaction with PX Developer.
• PX Developer Version1.40S or later
The following software is required to connect with GX Simulator.
• GT Designer3 Version1.105K or later *6 • GX Simulator Version5.00A or later
The following software is required to connect with GX Simulator2.
• GX Works2 Version1.12N or later
The following software is required to connect with GX Simulator3.
• GX Works3 Version1.007H or later
The following software is required to connect with MT Simulator2.
• MT Works2 Version1.70Y or later
The following software is required to connect with MELSOFT Mirror.
• MELSOFT Mirror Version 1.000A or later *15
The following software is required to use the OPC UA client connection.
• GT OPC UA Client
|
Other hardware | Use the hardware compatible with the above OS.
• For installation: mouse, keyboard, DVD drive
Prepare the following hardware if necessary.
• For execution: mouse, keyboard • For printing: printer • For execution (Only when outputting the buzzer sound): sound function, speaker
|
- *1Administrator authority is required for installing and using GT SoftGOT2000.
If you use GT SoftGOT2000 and other MELSOFT products simultaneously on the same personal computer, run the MELSOFT products with administrator authority as well. - *2The following functions are not supported.
• Activating the application with Windows compatibility mode
• Fast user switching
• Changing the desktop theme (or font size)
• Remote desktop
• Setting the size of text and illustrations on the screen to any size other than [Small-100%] - *3Tap and press-and-hold features are supported.
As operations such as flicking are not supported, the following operations are unavailable accordingly.
• Touching two touch switches simultaneously
• Moving an overlap window or key window by a slide operation
When [Allow press-and-hold of a mouse button to function as a right-click] is selected in the [Environment Setup] dialog of GT SoftGOT2000, the following operations are also unavailable.
• Touching a touch switch ([Action]: [Momentary])
• Touching a touch switch ([Delay]: [ON])
• Touching the utility call key - *4Operation in a virtual environment such as Hyper-V is not supported.
- *5When using GT Designer3 or PX Developer besides GT SoftGOT2000, additional free space is required.
For the available space required when using GT Designer3, please refer to the GT Works3 operating environment.
For the available space required when using monitor tool functions of PX Developer, refer to the following manual.
-> PX Developer Version â–¡ Operating Manual (Monitor Tool)
When using a user-created application, free space is required separately. - *6Use GT Designer3 included in GT Works3 that contains GT SoftGOT2000.
- *7The following OSs are not supported.
• Microsoft® Windows® 10 IoT Enterprise for Retail or Thin Client
• Microsoft® Windows® 10 IoT Enterprise for Tablets
• Microsoft® Windows® 10 IoT Enterprise for Small Tablets - *8The following lockdown features are not supported.
• Unified Write Filter
• Assigned Access
• USB Filter
• Layout Control
• AppLocker
• Shell Launcher
• Text cursor indicator - *9GT SoftGOT2000 (English version) is preinstalled.
- *10Microsoft® Windows® 10 IoT Enterprise 2016 LTSB is preinstalled.
For the specifications of the MELIPC, refer to the following.
• MELIPC MI5000 Series User's Manual (Startup)
• MELIPC MI3000 User's Manual
• MI2012-W User's Manual - *11Disable high-speed startup.
If enabled, GT SoftGOT2000 may not operate properly when the personal computer is shut down and then started. - *12Some digital pens are unusable.
- *13Only Desktop Experience is available.
- *14ARM64 and ARM32 are not supported.
- *15To run GT SoftGOT2000 and MELSOFT Mirror on the same personal computer, the operating environment of MELSOFT Mirror must be satisfied.
- *16Use the same language version of Windows OS as that of GT SoftGOT2000.
Ejemplo: When using the English version of GT SoftGOT2000, use the English version of Windows OS. - *17Install a language pack as needed.
[ Trademarks and registered trademarks ]
Microsoft and Windows are trademarks of the Microsoft group of companies.
Other product and company names are either trademarks or registered trademarks of their respective owners.