-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
Human-Machine Interfaces(HMIs)-GOT
Serie GOT Simple
- Feature
- Especificación
- Normas
- Discontinued
- Backup important programs
- Display industrial devices alarms
- Easily collect data from connected devices
- Increase efficiency of maintenance work
- Industrial devices data collection
- MODBUS® communication also supported
- Monitor device value and set values for timer, etc.
- Program change without a personal computer on-site
- Reduce mass production installation setup costs
- Related Link
- Mantenimiento remoto
- Setup and modification on-site
- Simple, easy-to-understand setup
- Use GOT SIMPLE to control industrial devices
Reduce design, setup, and maintenance cost
Reduce mass production installation setup costs
Start from SD memory card
Transfer the project data and all the necessary system data to make a GOT operate to an SD memory card in advance.
Then the GOT can be used just by inserting them. Useful for replacement or maintenance of GOT.
Industrial devices data collection
Función de registro
GOT manages the data of all connected industrial devices. The data can be collected at any arbitrary timing and can be used for data analysis and feedback.
The collected data can be displayed as a graph on the GOT, making it easy to understand temperature changes and other status updates at a glance.
Backup important programs
Backup/Restoration function
Programs of the programmable controller can be replaced even without a PC. When the programs and parameters are backed up to GOT*1, the data and machine operation can instantly be restored even if an unexpected failure occurs.
- *1A separate SD memory card is required.
- *2For details on connectable devices, please refer to the
Setup and modification on-site 

FA transparent function
Set up and modify devices without changing cable connections.
The GOT acts as a transparent gateway to enable programming, startup, and adjustment of Mitsubishi Electric industrial devices.
Mantenimiento remoto
Conexión ethernet
Office PC can connect to GOT on the factory floor for maintenance via Ethernet. With Ethernet, it is possible to connect a system of mixed vendors and models, expanding the possibilities at the factory floor. In addition, Ethernet printers*1 are supported so that the data (such as reports and screen images) can be printed by an Ethernet printer on the network, thus reducing hardware cost.
- *1For the connectable printers, please refer to the Technical Bulletin (GOT-A-0160).
Use GOT SIMPLE to control industrial devices 

Función de multicanal
GOT supports various industrial devices and connection types. With the multi-channel function, two channels of industrial devices can be monitored on a single GOT.
Easily collect data from connected devices
Device data transfer function
Using GT Works3, simply set source devices, destination devices, and triggers and you can transfer data between industrial devices. Data on the connected devices can be collected in the programmable controller without a sequence program.
MODBUS® communication also supported 
MODBUS® communication
As a master station, GOT can communicate with a MODBUS®/RTU slave device. Up to 31 devices (RS-485) can be connected for monitoring of production line, etc.
Simple, easy-to-understand setup
Recipe function & recipe display (record list)
GOT saves the recipe information (device values) such as material blend and machine conditions. You can change the recipe on the GOT and write it to a programmable controller to quickly perform the changeover. Changing recipes (changeover) is easy on a user-created screen or on the utility screen. The users can easily create screens by using the recipe display (record list).
Display industrial devices alarms
Función de alarma
Use the GOT to display and check alarms set by the users. Alarms of the connected device can be monitored and the equipment status can be checked. When a problem occurs, you can quickly troubleshoot the problem.
Increase efficiency of maintenance work
Reading/writing resource data
The GOT resource data can be read out to the PC, corrected, and then written back*1. The efficiency of maintenance work is enhanced as there is no need to exchange data with an SD memory card.
- *1For the details on resource data that can be read and written, please refer to the
Monitor device value and set values for timer, etc.
Device monitor function
Monitor and change internal device ON/OFF status, word values, timer and counter values of connected devices such as MELSEC programmable controllers.
Program change without a personal computer on-site
MELSEC FX list editor
With the GOT, sequence programs of FX Series programmable controllers*1 can be edited in the list format.
Convenient for minor on-site program changes.
- *1FX5CPU is not supported. For the details of connectable devices, please refer to the