-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
Human-Machine Interfaces(HMIs)-GOT
Serie GOT Simple
- Feature
- Especificación
- Normas
- Discontinued
Add value to your installation and machine
Security with password management
Operator authentication function
Setting the operation authority and the viewing authority per operator achieves "enhanced security" and "prevention of improper operation". Operator authentication can be performed startup and when the screen is switched.
Operation log function
The operation information, such as the "what, when, and how" of an operation performed can be recorded in chronological order in an SD memory card and checked on a PC.
In addition, when combined with operator authentication function, it keeps track of "who" has operated the device and quickly identify the cause of the trouble.
Easily exchange data with FTP
Función de transferencia de archivos
By using GOT, production results and alarm logs can be stored in an SD memory card of the GOT (FTP client) and sent to a PC (FTP server). The GOT can also receive the production instruction data from the PC.
By using the GOT as an FTP server, files can be read to and written from the PC that acts as an FTP client. (FTP server function)
Writing file from GOT to PC
Reading file from PC to GOT
Reduce risk of unauthorized access through network
IP filter function
Registering the IP address of the device which can access the GOT restricts the access from unauthorized devices.
Register the IP address of the device to allow access
Register the IP address of the device to prohibit access
Multiple actions with a single switch
Multiple functions can be set to one switch, so there is no need for multiple switches for separate functions. By setting execution sequence and conditions, delay, repeat, interlock settings can be combined, reducing the burden of programmable controller programming.
Easily installed on compact equipment
Pantalla vertical
By using a GOT vertically, it can be easily installed on compact equipment and can neatly display vertical letters.
Less scrolling is needed when displaying lists.