fa_logo

Controllers MELSEC-L Series

Product features -Analog/Temperature Control-

img-mv-1-sm
header_lup-md
analog-temperature-control-main-banner-sm

Easily and finely adjust the system startup time with the shift function

Shift function

Using this function, the set shifting amount to conversion value can be added (shifted) to the digital output value.
When the shifting amount to conversion value is changed, it is reflected to the scaling value (digital operation value) in real time. Therefore, fine adjustment can be easily performed when the system starts.

For L60AD4

■  Before adjustment

Input voltage (V) Valor de salida digital
0 -10
5 19990

point_img01_arr

■  After adjustment

Input voltage (V) Valor de escalamiento
(digital operation value)
0 0
5 20000

Reduce the time taken for programming

Scaling function

The scaling function converts values directly to easy-to-understand units without requiring any programming.
Since a separate conversion program is not required, the number of overall programming steps can be reduced.

Scaling settings example (L60AD4)

Normally an analog input of 4 to 20 mA is converted to a digital value from 0 to 20000. Using the scaling feature, the same input can result in a digital value of ±20000.

point_img02a-mdpoint_img02a-md
Corriente de entrada (mA) Valor de salida digital Valor de escalamiento
4 0 -20000
8 5000 -10000
12 10000 0
16 15000 10000
20 20000 20000

Digital filtering function

This function eliminates unnecessary frequency elements with simple parameter settings. Select from low pass filter, high pass filter or band pass filter.
Programming steps can be further reduced as extra ladder code is not required to achieve the filter processing.
The filtered A/D conversion program is available at the same time as conversion completion, reducing the overall conversion to filter process time.

point_img02b
point_img02c

First-delay filter function

The first-delay filter function constant outputs a digital value which filters out (smooths) the excessive noise.

Log data for up to 10.000 points

Función de registro

Data is continuously collected at the set cycle and stored in the buffer memory.
Data stored in the buffer memory can be used for debugging, and to periodically confirm data variations.

Artículo Descripción
L60AD4 L60AD2DA2
Collectable points 10000 puntos/canal
Collectable data Digital output value or scaling value(digital operation value)
Logging cycle*1 80...32767µs
1...32767ms
1...3600s
80...32767µs
1...32767ms
1...3600s
Conversión de velocidad 80 µs, or 1 ms 80 µs
Level trigger condition Above, Below, Pass Through
Logging points after trigger 1...10000
  • *1.The actual logging cycle is"an integral multiple of the conversion cycle of each A/D conversion method".
    Ex.) When using the sampling processing: Conversion cycle = conversion speed × number of channels in use.

The logging data can be analyzed with the GX LogViewer.

When an error is detected in the digital value:

point_img03a-md

Logging data can be transferred to the CPU device memory while still logging.
Logging and data transmission can be executed simultaneously so the next logging session can be started right away.

Logging for 10.000 points and greater

When logging of 1001 - 2000 points of data commences, the first 1000 points (1 - 1000) are stored into the CPU device memory. By storing every 1000 points of data in the CPU, overall logging of total data larger than 1000 points can be logged.

point_img03b

Easily measure part thicknesses!

Difference conversion function

When the difference conversion starts, the scaling value (digital operation value) at that time is determined as the difference conversion reference value. The value acquired by subtracting the difference conversion reference value from the scaling value (digital operation value) is stored as the scaling value (digital operation value) after difference conversion.

point_img04

Scaling value (digital operation value)
after difference conversion
= Scaling value
(digital operation value)
- Difference conversion
reference value

Extend the detection method according to applications

Input signal error detection extension function

Using this function, the detection method of the input signal error detection function can be extended. Use this function to detect an input signal error only at the lower or upper limit, or to execute the disconnection detection.

Input range extension function

The input range can be extended. By combining this function with the input signal error detection function, simple disconnection detection can be executed.

Connected devices monitoring alarm

Warning output function

■  Process alarm
Outputs an alarm when the digital output value enters a preset alarm range.

module-features/point_img06a

■  Rate alarm
An alarm is generated if the digital output value's variation rate is larger than the rate alarm upper limit value, or if it is smaller than the rate alarm lower limit value.

point_img06b

Noise isolation for smoother system operation<sup>L60AD4-2GH</sup>

Channel isolation

Each channel is isolated preventing any noise interference between channels resulting in more stable measurements.

point_img07

A/D variable conversion timing

Trigger conversion function

A/D conversion is processed at the rising edge of the trigger position timing.
This function enables easier use of the converter and enhances the overall program performance.
There are two types of trigger conversion request:"External trigger conversion request (external input terminal)" or"internal trigger conversion request (buffer memory)".

point_img08a
point_img08b
  • *2.Carried out in order with combination of channel 1, channel 3 and channel 2, channel 4.

Quickly calculate and record flow amount

Función de integración de flujo de cantidad

This function performs the A/D conversion of analog input value (voltage or current) from a flow meter and others, and integrates the scaling value (digital operation value) by every integration cycle. In this function, integral processing is performed regarding the scaling value (digital operation value) as the instantaneous flow amount.

■  Concept of integral processing
With this function, integral processing is performed using the following formula.

point_img09a
point_img9b
Artículo Descripción
Integrated flow amount Result of integral processing
Instantaneous flow amount Instantaneous flow amount value output in analog from flow meter
ΔT Integration cycle (ms)
T

Conversion value to convert time unit of instantaneous flow amount to ms unit

Range of flow meter Setting value to specify flow amount time unit T (ms)
/s 0 1000
/min 1 60000
/h 2 3600000
Unit scaling

Unit scaling for integrated flow amount
This is used when the value of instantaneous flow amount × ΔT/T is 0 to 1.

Setting value to specify unit scaling Unit scaling
0 1
1 10
2 100
3 1000
4 10000
Previous amount Stored integrated flow amount value before integral processing

Realize fast and smooth continuous analog output

Wave output function

The industry's first*3 waveform output function is included.
This function enables control wave data that is faster than the program control to be directly registered in the D/A converter module and output the data at a set conversion cycle.
Therefore, the analog output value is not affected by the scan time of the CPU module resulting in faster and smoother analog control.

  • *3.Mitsubishi Electric survey dated April 2012.

Analog output from sequence program

Analog values are output at each scan time.

point_img10_a

The actual waveform and the output waveform deviate.

point_img10_arr

Analog output with waveform output function

Analog values are output at set interval.

point_img10b

The output waveform is closer to the actual waveform (less deviation).

The actual waveform and the output waveform deviate.

point_img10_arr

The output waveform is closer to the actual waveform (less deviation).

  Using GX Works2 to create the waveform output data to be analog output

point_img10c

By registering the waveform patterns (multiple), they can be combined freely with the tool.

 Save waveform output data into CPU module's file resister (or SD memory card)

point_img10d

 Execute the function block (FB)*4 and register into analog output module

point_img10e
  • *4.Contact your local Mitsubishi Electric sales office or representative.

More flexible calculation and conversion reduce programming time<sup>L60AD2DA2</sup>

Conversion by polynomial expressions

The variable arithmetic function enables the analog I/O module to perform polynomial calculations, eliminating the need of such calculations programmed by ladder. With the calculations performed on the analog I/O module side, advanced calculations are possible without being restricted by the scan time.

point_img11a

Graph-form conversion characteristics

The variable conversion characteristics function enables conversion characteristics for analog input, analog output, and analog I/O to be easily set on graphs. This means that conversion characteristics do not need to be programmed by ladder, which leads to reduced programming time.

Artículo Descripción
Entrada analógica Conversion characteristics can be easily set for the A-D conversion channels (CH1, CH2).
Rango de Conversion characteristics can be easily set for the D-A conversion channels (CH3, CH4).
E/S analógica Conversion characteristics for the analog input-output conversion can be easily set in simple steps, eliminating the need of creating ladder programs.

Previous control method

Ex.) Analog output module

point_img11b

Control using graph-form conversion characteristics

Ex.) Analog I/O module

point_img11c

Conversion by graph-form conversion characteristics plus polynomial expressions

The two functions described above can also be combined; the digital values are first converted according to graph-form conversion characteristics and then by polynomial expressions. These two levels of conversion realize full adjustment of analog values at the time of output rather than adjusting them post-conversion.

Ex.) Obtaining intended analog output using the conversion by graph-form conversion characteristics plus polynomial expressions

point_img11d
point_img11e

One module covering voltage, current, micro-voltage, thermocouples and RTD

For each channel, it is possible to select from voltage, current, micro-voltage, thermocouples or RTD. As a result, dedicated modules required for each type of sensor can now be integrated into a single module.

ExampleSystem with up to four channels (including analog and temperature input channels)

point_img12-mdpoint_img12-md

The multiple input module also supports the Pt50 and JPt100 sensors, which are compatible with the former JIS standards. Modules can be replaced without altering the already existing sensor equipment.

Termopar K, J, T, E, N, R, S, B, U, L, PL Ⅱ, W5Re/W26Re
RTD Pt1000, Pt100, JPt100, Pt50

8 input channels with wider input ranges<sup>L60RD8</sup>

Single L60RD8 can measure temperatures of up to 8 channels. With the number of supported channels doubled compared to before (L60MD4-G), space and cost savings can be realized. The input range is expanded to meet the DIN standards, GOST standards, and Pt1000 range in addition to Pt100, JPt100, and Pt50, bringing new application possibilities.

RTD Pt1000, Pt100, JPt100, Pt50, Ni (DIN standards), Cu (GOST standards)

Reduced wiring time with no screw tightening<sup>L60RD8</sup>

The module is equipped with a spring clamp terminal block, which does not require screw tightening. This push-in type terminal block does not require any dedicated wiring tool and significantly reduces the installation time.

point_img14

Easier calibration<sup>L60RD8</sup>

Measured temperatures can be easily calibrated towards the actual temperature using the sensor calibration function (shift function, 2-point sensor compensation function).

point_img15

The measured temperature of 10,8 to 50,7 (°C) is calibrated to be 10,5 to 50,0 (°C) by digital calculation. A temperature closer to the one input to RTD is obtained.

Powered by Translations.com GlobalLink Web Software