-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
Programmable Controllers MELSEC-A Series
Renewal
Use I/O combined module without program change when replacing AH42/A0J2(H) CPU
Upgrade exampleModules for Easy Replacement
Supported series:
Plentiful Q Series modules facilitate the replacement
I/O combined module * A module with sequential I/O numbers
QX41Y41P's I/O assignment is the same as that of the A/QnA Series I/O combined module, AH42. This module can be used as the I/O module on the programmable controller side when using A0J2 Upgrade Tool (manufactured by Mitsubishi Electric System & Service Co., Ltd., refer to page 23) to replace the A0J2(H)CPU.
It is not necessary to change the programs when replacing AH42 or A0J2(H)CPU. (Minimize the need to modify programs)