-
Consultas
-
Seleccionar
y cotizar -
Compartir
-
Socios
Programmable Controllers MELSEC-A Series
Renewal
Discontinued products
We would like to inform you regarding the models of the A/QnA Series and the AnS/QnAS Series of products that have been shipped since their launch in 1985, for which production has been terminated, as well as those for which production will continue, as described below. We ask for your understanding.
Discontinued products | Date of discontinuation |
Servicio disponibilidad periodo |
Técnico Bulletin |
|
---|---|---|---|---|
Large type A Series/ Large type QnA Series |
|
End of Sep. 2006 | End of Sep. 2013 | T99-0050 |
|
End of Sep. 2014 | End of Sep. 2021 | FA-A-0141 | |
Small type AnS Series/ Small type QnAS Series |
|
End of Sep. 2008 | End of Sep. 2015 | T99-0049 T99-0070 |
|
End of Sep. 2014 | End of Sep. 2021 | FA-A-0142 | |
|
End of Mar. 2019 | End of Mar. 2026 | FA-A-0260 | |
|
End of Mar. 2023 | End of Mar. 2030 | FA-A-0364 | |
●Power supply module (A1S61PN, A1S63P) | End of Apr. 2024 | End of Apr. 2031 | FA-A-0411 | |
●Large capacity battery unit (A10BAT) | End of Apr. 2024 | End of Apr. 2031 | FA-A-0405 | |
A2C Series |
|
End of Sep. 2006 | End of Sep. 2013 | T99-0050 |
|
End of Sep. 2008 | End of Sep. 2015 | T99-0070 | |
Network interface board |
|
End of Sep. 2008 | End of Sep. 2015 | T99-0049 |
AOJ2(H) Series |
|
End of Sep. 2008 | End of Sep. 2015 | T99-0069 |
Módulo de E/S remoto |
|
End of Sep. 2008 | End of Sep. 2015 | T99-0070 |
|
End of Sep. 2014 | End of Sep. 2021 | FA-A-0142 | |
Serie Q |
|
End of Sep. 2022 | End of Sep. 2029 | FA-A-0315 |
Models in continuous production
The production of the A/QnA Series products except the following modules has been discontinued since September 2006.
Nota: In accordance with the continuation of production, model names may be changed.
Tipo | Modelo |
---|---|
Large type A/QnA Series power supply module*1 | A61PN*2 |
A61RP | |
Batería | A6BAT |
A8BAT |
- *1.If using power supplies other than the above, please consider switching over to one of the above models.
- *2.A61PN is a replacement of A61P/A61PEU/A61P-UL.
Only some models of the MELSEC-A/QnA (Large Type) Series are still in limited production. However, the EN61131-2:2003 certification has expired, so the CE Declaration for models still in production has been withdrawn.